Portescap in Motion

Seeing beyond what's in the catalogue

Posted by Valentin Raschke   Nov 16, 2020   0 Comments

Seeing beyond what's in the catalogue: Why it's important to get in touch with Portescap

Finding the right motor can be a challenge. Often a product catalog only lists a selection of available motors and coils, so the ideal solution can't be found by browsing through available standard options. Some motor manufacturers offer customizations, which require time and money to be invested and might not always be an option depending on the size of the project.

Read More

Topics: Others

Dual Motion Can Stack Actuator

Posted by Daniel Muller   Nov 03, 2020   0 Comments

Portescap's Innovative Dual Motion Can Stack Actuator Solution

Rotary and Linear Motion in One Compact Solution

Some applications require rotary motion, such as ventilators. Others require linear motion, such as medical pipettes or syringes. When it comes to combining a rotary and a linear motion in the same application, designers often need to integrate 2 motorized solutions so they can control both degrees of freedom (rotation and linear) at the same time.

Read More

Driving DC Brushed Motors

Posted by Chris Schaefer   Sep 04, 2020   0 Comments

Driving DC Brushed Motors

To control a DC motor, a variable, and controlled power supply is needed. There are three types of methods that can be used:         

    • Voltage-controlled linear supply
    • Current linear supply
    •  PWM (Pulse Width Modulation)
Read More

Brushless DC Motors Let You Avoid Having To Compromise On Performance For Low Voltage Battery Powered Tools

Posted by Guillaume Mougin   Aug 11, 2020   0 Comments

Today’s most challenging battery-operated tools require power, speed, and efficiency within the most ergonomic package. Studies have proven that users prefer a smaller and lighter tool with a high level of performance. The ergonomics needs have tremendously increased in the last few years to highlight operator comfort and efficiency while using battery-powered tools.  

There are multiple ways to lighten the tool. For example, we recognize the battery of the tool as one of the heaviest components, therefore the trend is to reduce the battery size. Lowering the battery size will affect the number of cells and thus the voltage: The smaller the battery, the lower voltage.

Industrial power tools support the increase in productivity while remaining versatile. We achieve productivity gains thanks to faster working cycles, so the tool should deliver higher speeds. We derive versatility from an increased torque capacity. 

Read More

Why An Encoder?

Posted by Chris Schaefer   Jun 16, 2020   1 Comments

Encoders provide feedback for accurate control of speed and positioning. The rotor angular position is given through two square waves 90 degrees shifted and an optional index pulse occurring once a revolution. There are multiple technologies to get these results.

Read More

Fight COVID-19 Together

Posted by Sandra Mehdian   May 18, 2020   0 Comments

Portescap is working closely with our customers to continue to provide miniature motors and precision motion control solutions for medical devices and clinical diagnostics which are essential to the fight against Covid-19. Portescap has been a leading expert in miniature motors and precision motion control solutions for medical devices and clinical diagnostics for many decades and we’re proud to be able to play an important role during this crucial time.  Brushless DC motors and brush DC motors are vital for life-saving medical devices.   

Read More

Topics: Medical & Diagnostics

Selecting the Optimum Motion Technology for Your Application: Motor Decision Table

Posted by Dave Beckstoffer   Apr 01, 2020   0 Comments

Decision-Tree

 

As this series has shown, there are many factors to consider when choosing the optimum motion technology for your application.  Your application may have one or more primary factors, which would provide a starting point based on the best technology for that factor or factors.  But reviewing all the factors and how they impact the final product output will enable the ideal performance of our product.  Below is a summary table for the factors and the three motor technologies:

Read More

Selecting the Optimum Motion Technology for Your Application: Type

Posted by Dave Beckstoffer   Feb 14, 2020   0 Comments

application-type

The type of application being designed will dictate different factors be considered for the motion solution.  Will the product be stationary?  Is the product mobile - being moved by an apparatus or on a person?  The typical usage of the product brings forth different factors to prioritize for your motion solution.

Read More

Topics: Others

Ultra EC High Performance Motors  For Battery-Operated Power Tools

Posted by Portescap   Feb 03, 2020   0 Comments

Our Ultra EC motors have been designed to meet the needs of Industrial Power Tool, watch our new video to learn more!

 

Read More

Meet Our Newest Innovation: Ultra EC™ Proprietary Coil

Posted by Portescap   Jan 24, 2020   0 Comments

The core of the Ultra EC™ platform is the innovative and proprietary U coil design which powers the performance of all 3 Ultra EC product lines. Watch this video to learn more about its features and benefits.

 

Read More

Meet The Family: Ultra EC Brushless Motors

Posted by Portescap   Jan 10, 2020   0 Comments

Our new Ultra EC Brushless Motors video highlights Portescap's Ultra EC three families of motors along with their features and benefits. Watch our latest video to learn more about our Ultra EC Product line. 

Read More

Topics: Automation, Others

Selecting the Optimum Motion Technology for your Application: Duty Cycle

Posted by Dave Beckstoffer   Dec 04, 2019   0 Comments

The next factor to review is the duty cycle for the motion solution in the application.  The duty cycle is defined as the ratio of the time the motor operates divided by the amount of total time for the cycle.  Typically, the motor does not run continuously but rather operates for a period (on-time) and then rests for a period (off-time).  The duty cycle affects the selection of the optimum motion solution, so it is important to understand the details and factors to consider.

Read More

Topics: Others

Day of Caring: Innovation from Within

Posted by Sandra Mehdian   Oct 28, 2019   0 Comments

The definition of innovating is to make changes to what is already establish. At Portescap we are always innovating, improving upon our processes and products to add value. Community organizations across the country are doing the same thing, they are changing our community and our world by building upon what is established. A Day of Caring is an opportunity where our team of innovators can come together with community innovators to help make our community a better place. 

Read More

Topics: Others

Experience How Portescap Surgical Motors Team Can Help You Find Solutions!

Posted by Sandra Mehdian   Sep 20, 2019   0 Comments

Our new Surgical Motor video highlights Portescap's innovative strengths and expertise in Surgical Motors Solutions. Press play and learn more about Portescap's mini motors technology, why you should work with us, and our approach to design and collaboration. The Surgical Motors Team also highlights our customization process and maps out our typical lead times. Call us today to experience how we can work with you hand-in-hand to find the optimal motor solution for your application!

Read More

Selecting the Optimum Motion Technology for your Application Series: Accuracy

Posted by Dave Beckstoffer   Sep 06, 2019   0 Comments

Another factor to review is the accuracy required from the motion system in the application.  Is the motion continuous or incremental?  What is the resolution needed from the motor during incremental operation?  Does the motor need to have different resolutions for different points in the operation?

Read More

Topics: Others

Selecting the Optimum Motion Technology for your Application Series: Mechanical Envelope

Posted by Dave Beckstoffer   Aug 21, 2019   0 Comments

The next factor for consideration is the mechanical envelope for the motion system.  What is the space in the product that is dedicated to the motion system?  Is there flexibility on the diameter or length?

Read More

Topics: Others

Selecting the Optimum Motion Technology for your Application Series: Lifetime

Posted by Dave Beckstoffer   Jul 19, 2019   0 Comments

The next factor we will consider is the lifetime requirement of the motion system.  How many cycles must the motion system execute within the life of the product?  How many hours does that require from the motion system?

Read More

Selecting the Optimum Motion Technology for your Application Series: Torque

Posted by Dave Beckstoffer   Jun 28, 2019   0 Comments

The next factor we will consider is the output torque requirement of the motion system.  What is the continuous torque requirement during operation?  Is there a peak torque for a limited time that needs to be considered?  Is the safety margin enough to compensate for the other factors in the application? 

Read More

Selecting the Optimum Motion Technology for your Application Series: Speed

Posted by Dave Beckstoffer   Jun 06, 2019   0 Comments

One of the first factors to consider in your new product development is the output speed requirement of the motion system.  How fast does the motor need to rotate to drive the mechanism in the application?  And are there various speeds that need to be accommodated?  There are some general guidelines that will help you narrow down the technologies to consider:

Read More

A Balancing Act

Posted by Christina Heston and Nate Schutte   May 16, 2019   1 Comments

What is rotor balancing?

Rotor balancing is the process of bringing the mass center axis of a rotor in line with the rotor’s shaft axis, within certain industry balance standards. A rotor, balanced or unbalanced, wants to revolve around its mass center axis. The balancing process brings these two axes together. As illustrated below, when the mass that causes the imbalance is removed, the two axes merge.

 

Read More