Portescap in Motion

Motion System Options for HVAC Gas Valve Actuators

Posted by Mahesh Dundage   Feb 21, 2022

Motion System Options for HVAC Gas Valve Actuators

In HVAC systems that provide heat for enclosed spaces, gas and liquid flow must be controlled and metered accurately using sensing and modulating elements such as flow control valves or isolation valves. Some control valves are opened and closed manually at the valve stem, while electronic valves incorporate an actuator to move the stem with control from a motor and drive system. Designers have three motor types to choose from, depending on the application requirements. Here’s a summary of the motion system options:

Read More

Topics: Stepper Motors, brushed DC motors, Portescap, DC motors, motor selection, electric damper actuators, HVAC systems, HVAC, gas and liquid flow, fluid control, linear stepper motors, actuators, HVAC gas valve actuators, position system, rotary motion, linear motion, closed loop positioning

Improve Thermal Performance for Ironless Brush DC and Brushless DC Motors

Posted by Daniel Muller   Dec 20, 2021

Improve Thermal Performance for Ironless Brush DC and Brushless DC Motors

Electric motor manufacturers must ensure that a motor’s instant internal temperature never exceeds its various components’ maximum allowable temperature. Depending on the design of the motor and the materials used, thermal phenomena will dictate the motor’s performance. Motor designers typically have two options to enhance motor performance without overheating and damaging its components: increase power conversion efficiency by generating less heat for a given mechanical power output or improve the motor's cooling capability through heat dissipation.

Read More

Topics: brushed DC motors, Portescap, Brushless DC motors, DC motors, iron losses, power conversion, heat dissipation, spotless brushless motors, motor design, thermal management, power losses, temperature rise, steady state operation, heat transfer, thermal resistance, excessive temperature, electrical resistance, thermal conductivity, transient operation, peak torque, periodic duty cycle

What to look for in a Miniature Motor when Designing your Next Robotic Application

Posted by Portescap   Oct 20, 2021

What to look for in a Miniature Motor When Designing Your Next Robotic Application

Advancements in automation and artificial intelligence are driving innovation in robotics. New developments in vision systems and sensor technologies require inventive applications for robots in the medical, warehousing, security and process automaton fields. These disruptive technologies are are creating new opportunities for miniature motors in the medical, warehousing, security and process automation fields.

Read More

Topics: Automation, Robotics, electric motors, brushed DC motors, brushless DC coreless

Subscribe to Email Updates

Posts by Topic

see all

Follow Us