Portescap in Motion

Motion System Options for HVAC Gas Valve Actuators

Posted by Mahesh Dundage   Feb 21, 2022

Motion System Options for HVAC Gas Valve Actuators

In HVAC systems that provide heat for enclosed spaces, gas and liquid flow must be controlled and metered accurately using sensing and modulating elements such as flow control valves or isolation valves. Some control valves are opened and closed manually at the valve stem, while electronic valves incorporate an actuator to move the stem with control from a motor and drive system. Designers have three motor types to choose from, depending on the application requirements. Here’s a summary of the motion system options:

Read More

Topics: Stepper Motors, brushed DC motors, Portescap, DC motors, motor selection, electric damper actuators, HVAC systems, HVAC, gas and liquid flow, fluid control, linear stepper motors, actuators, HVAC gas valve actuators, position system, rotary motion, linear motion, closed loop positioning

Subscribe to Email Updates

Recent Posts

Posts by Topic

see all

Follow Us