Improve Thermal Performance for Ironless Brush DC and Brushless DC Motors
Electric motor manufacturers must ensure that a motor’s instant internal temperature never exceeds its various components’ maximum allowable temperature. Depending on the design of the motor and the materials used, thermal phenomena will dictate the motor’s performance. Motor designers typically have two options to enhance motor performance without overheating and damaging its components: increase power conversion efficiency by generating less heat for a given mechanical power output or improve the motor's cooling capability through heat dissipation.