Portescap in Motion

Portescap’s Brushless Slotted DC Motor Testing Capabilities

Posted by Andrew Sharp

Sep 20, 2016

Portescap’s miniature motors are often used by medical tool and device manufacturers and OEMs, in highly demanding end applications. An in-house testing process is sometimes required to further validate and confirm the design process. We’d like to give you a glimpse into Portescap’s motor testing capabilities for brushless slotted DC motors.

Read More

Topics: Medical & Diagnostics, Automation

MotionCompassTM – Selecting the “right” motor for your application

Posted by Vinicius Cabrera

Jun 15, 2016

 

Are you an original equipment maker [OEM] looking for a specific motion control solution for your end application? Portescap caters to miniature motor requirements of a wide range of medical, diagnostic and industrial applications. This ranges from medical and surgical tools, lab automation equipment, dental drills and textile yarn guides to humanoid robots, surveillance camera systems, aircraft seat actuation, tattoo machines, and more. We help OEMs select the “right” miniature motor to power their applications. Our solutions include miniature dc and bldc motors, miniature can stack steppers and disc magnet motors as well as linear actuators with gear composite. These are usually customized to varying degrees, to suit requirements of the end application.

Since our motors are exposed to diverse operating conditions, selecting the right motor can be a daunting task. Certain applications need motors that can operate at extreme temperature ranges, whereas in some cases, OEMs are looking for motors with ability to withstand shocks and vibrations. Parameters like “length”, “diameter”, “torque”, “speed”,  “power density” etc  play an important role in motor selection. Thus, we’ve provided our clients and prospects with an online platform - MotionCompassTM, that helps them select the best-suited motor for their application.

 

Read More

Topics: Medical & Diagnostics, Automation, Others

Understanding Speed-Torque Characteristics of Miniature DC Motors (Part 2 of 3)

Posted by Sandeep Gandre

May 23, 2016

Read: Part I

[continued...]

Now we shall consider the motor speed against an application. We need a motor such that higher limit of its permissible speed should be higher than the operating point of the application. Maximum permissible limit corresponds to upper limit of operating range diagram. This speed limit can be found in our catalogue.

Read More

Topics: Medical & Diagnostics, Automation, Others

Understanding Speed-Torque Characteristics of Miniature DC Motors (Part 1 of 3)

Posted by Sandeep Gandre

May 17, 2016

Portescap offers miniature motor technologies to solve the motion needs of end markets. Our typical markets can range from motors for medical devices to various industrial applications. We serve our customers through innovative product technologies encompassing brushless miniature DC motors, brush DC & can stack motors, disc magnet motors and stepper linear actuators, to optimize their application performance.

Read More

Topics: Medical & Diagnostics, Automation, Others

Miniature Disc Magnet Motors for Textile Applications

Posted by Norbert Veignat

Mar 14, 2016

 

In the 80’s, Portescap was mainly involved in the watch industry providing small stepper motors to be used in watches and clocks. Using rare earth magnets, we then designed the first micro motor with a multipolar structure. Such a design avoids additional pole shoes on the rotor to create fewer steps per revolution. Later, Portescap expanded its expertise to include bigger motors for industrial applications [< 100 W].

Read More

Topics: Automation, Others

Miniature Motors for Medical Devices and Dispensing Systems

Posted by Portescap

Jan 11, 2016

 

Health care safety is now a top priority and concern among health care practitioners and consumers. In today’s medical devices marketplace, the demand for reliable and safe medical devices and equipment comes not only from the clinical end user, but also from informed patient consumers.

For those involved in the development and manufacture of medical devices and equipment, the demand for safety and quality brings with it new and exciting challenges. How does one build equipment and devices that meet the hundreds of stringent needs of the clinical end user and health care consumer? How does one decide with whom to partner in this far-reaching world of device and equipment manufacturing?

Care givers constantly need products that assist them in achieving the best possible clinical outcomes for their patients. Where do we get motion control solutions, i.e. motors for medical OEMs capable of navigating the demands of the health care industry?

Read More

Topics: Medical & Diagnostics, Instrumentation, Automation

Portescap Introduces New P532 Motor Series for Best-in-class Power Rate and Acceleration

Posted by Dave Beckstoffer

Dec 21, 2015

Portescap has recently introduced the P532 Series Disc Magnet Step Motor with encoder to deliver best-in-class motor acceleration and power rate and thus outperform the standard Brushless DC motor in a wide range of applications.

Stepper motors typically run at 2,000 RPM or less in an open loop, while brushless motors that can run at much higher speeds are typically used in closed loop applications. In the last few years, trend is to use a stepper motor in closed loop with a torque higher than a brushless motor system, because of its higher pole count. What we are typically looking at is the middle range of revolutions per minute [RPM] as a sweet spot for disc magnet motors. The sweet spot opens up in applications in the few thousand RPM range, where a closed loop disc magnet motor system can be more cost-effective than a brushless solution.

Read More

Topics: Medical & Diagnostics, Instrumentation, Automation

Stepper Linear Actuators Simplified

Posted by Portescap

Oct 27, 2015

What is a “linear actuator”? It is actually a simple stepper motor with a built-in leadscrew to directly convert rotary motion in form of discrete steps, into linear motion. Achieving linear motion internal to the motor eliminates the cost of designing a separate transmission mechanism in the system.

Read More

Topics: Security & Surveillance, Medical & Diagnostics, Instrumentation, Automation, Others